Hi,
i'm developing a boost converter using the TPS61175.
My project is based on the TPS61175EVM-326.
The EVM uses a inductor (part number CDRH105RNP-220N) from Sumida Inc.
I'm with dificulties to find this model to buy, but I found the part number CDRH104RNP-220NC.
It is very similiar, but the DC resistance is a bit higher.
My Vin is between 3 - 12V and Vout = 12.
Could I use the CDRH104RNP instead of CDRH105RNP smoothly?
Thanks,
Cláudio