Hi,
I hope I'm right here. I have question concerning the TPS2020:
Datasheet says that output voltage must not be higher than input voltage by more than 0.3V:
http://www.ti.com/lit/ds/slvs175c/slvs175c.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I hope I'm right here. I have question concerning the TPS2020:
Datasheet says that output voltage must not be higher than input voltage by more than 0.3V:
http://www.ti.com/lit/ds/slvs175c/slvs175c.pdf
It's referring to an enabled TPS2020 with an input source, Vin, and the output connected to a source Vin + 0.3V. This is done to protect ESD structures designed to withstand transient but not excessive DC voltage. TPS2020 will survive the examples you gave because the part is diabled or has input voltage removed.
Hi Bob,
thanks for your fast response, I appreciate it!
So, if a sudden and heavy short at the input can occur, leaving the TPS2020 still enabled for a brief period, would you say it is better to have an external protection diode from output to input to protect the internal ESD protection scheme? Would a Schottky diode be sufficient then?
Kai