I am trying to replace a very old power supply that is composed of 2 seperate internal switching power supplies. One side of the power supply has a +26VDC input with a +20VDC output at 1.5A. The othe side of the power supply is the exact opposite, -26VDC input with a -20VDC output. I would like to know if it's possible to use a LMZ14202H with the negative voltage input. The datasheet does state "Negative voltage output applications" but is rather silent beyond that statement.