Hi,
I have selected INA138 high side current monitoring IC from TI.
I have attached the typical scheme for current monitoring planning to implement.
1) I need to monitor the current flowing in -8000V line which is w.r.t GND. The peak current is 270mA for 20% duty.
2) One more IC will be used for monitoring the current in 100V line whicj is w.r.t -8000V. The peak current is 20mA for 20% duty.
Also i will be generating one +5V supply w.r.t -8000V and this supply will be used for IC functionality.
Whether the above said will work. If not, suggest some monitoring scheme.
Regards,
Santhakumar.S