Other Parts Discussed in Thread: TPS40210, TL783, TL431
Hi,
I used TPS40210 to generate +100V and -100V outputs in my circuit, it works fine but switching noise on output is as high as 1V~2V, which is not acceptable for my application.
I had tried to add RC filter on both outputs, switching noise can be reduced a little bit but still not acceptable.
Then I add a positive LDO(TL783) on +100V output and reduce output voltage to -90V, the switching noise on +90V is much more reduced(about 300mV), so I think a suitable LDO can help me to overcome switching noise problem.
However, I cannot find a LDO which can accept -100V input and output -90V. Is there any way to use existing LDOs with some modifications(cascading LDOs?) to achieve this application ?
P.S. output loading is about 100mA for both +90V and -90V
Thanks a lot.