Hello,
I use in our application the TPS76201 LDO regulator. I want to regulate the LDO with a 10K ohm digital potentiometer in the range of 0.7 V to 5.5 V (VOUT - 10K digital poti - GND). According to the datasheet are Low resistors in the feedback-pin allowed. But when low resistance regulates the LDO, I don't have a high resolution (50mv resolution nedeed) or the LDO dont work properly. And by high resistance the ldo have a high resolution. Works the TPS76201 linear? Can you suggest us, or a Alternatively LDO?
Thanks.