Q: Is there a TPS62410 EVM orderable on the web?
A: No but the TPS62410 and TPS62420 have the same package and pinout. Therefore, you can remove and replace the TPS62420 IC on the TPS62420EVM-167 with a TPS64210 IC. Note that the inductor on TPS62420EVM-167 may not be rated high enough for an application using the TPS62410 and so the inductor may need to be replaced. There are no plans to develop a dedicated EVM for the TPS62410.