This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sharing the thermistor between gas gauge and charger

Other Parts Discussed in Thread: BQ24050, BQ27200

Hello- We plan to use the BQ24050 charger with the BQ27200 gas gauge (system side). Is there a way there two device can share the thermistor in the battery? Thanks!

-Tim Starr on behalf of VC@AR

  • Sharing the thermistor in the battery by both charger and gauge is not impossible, but is very tricky, and not recommended.  You will have to synchronize and isolate the measurement, two measurements at the same time will produce an incorrect temp reading. The biasing circuits are different, so the same thermistor cannot be connected to both ICs without using isolation, such as with an analog switch. 

    Connect the battery thermistor to the gauge to ensure the accurate temperature measurements of the cell for accurate gauging.  The gauge also uses the thermistor for detection of battery insertion and removal. If you don't want to add a thermistor for the charger, then connect the fuel gauge BAT_GD pin to the charger CE pin. 

    -Leonard

  • In the case of the BQ27200, it does not need an external thermistor.

    The bqJUNIOR uses an integrated temperature sensor to monitor the pack temperature and is reported through
    the internal registers. The temperature measurement is used to adjust compensated available capacity and
    self-discharge capacity loss.

    The BQ24050 does need an external thermistor.