Other Parts Discussed in Thread: TPS55340, LMV431, LM3481
Hello, I need to design a LED backlight driver with some uncommon features (input voltage 5V, output voltage 15...25 V with constant currents up to 1A). Since I'm not finding a LED driver that fullfills my needs, I'm considering to use a generic boost converter instead, e.g a TPS55340. The idea is to connect the FB input (normally used for the voltage feedback loop) to a sense resistor in series with the LED string. I've already seen some thread regarding this, I just wanted to make sure that this is a safe technique and there aren't any vicious pitfalls to avoid.
Thank you!