Hello,
for the TPS2500/5 Let’s assume the following scenario:
- USB OTG port functions as B-device (doesn’t source current);
however, no power is drawn from the USB bus
- Boost converter is enabled and AUX output is used to power other devices on board
- USB switches are disabled (ENUSB=0)
- The USB port is connected to a host (A-device) which provides 5V on VBUS which is connected to USB pin of TPS2500
- Voltage on USB pin is larger than AUX output: VUSB > VAUX
My questions are:
- Can there be a reverse current flow from USB pin to AUX pin?
- What if VUSB > VAUX x 1.05? Can it trigger the AUX OVP?
- Is there a minimum value for VOVP? Datasheet gives only a typical value.
Thanks,
Ran