Other Parts Discussed in Thread: TL494
I have inherited an old power supply design using a TL494 driving the primary of a transformer in push-pull mode. Recently we have had several board that when VCC power is applied the TL494 output transistors just won't start switching. The Osc at pin 5 always starts when VCC is applied and all the control voltage seem correct. But the output may not start switching for a few mSec to several minutes. If power is turned off and then back on quickly everything looks normal but if power is left of for a few minutes the part is likely to be latched up again.
All the failed units have the same date code '32C3NRK'. Has this been reported as a questionable lot? This design did not use the soft-start, DTC is tied to ground and they are pushing a 4.4v level pulse signal into the feedback pin 3 to stop switching while some sensitive signals are measured. I don't like that approach, but I also don't see why that should be causing the problem.
Any suggestions?
Thanks
Maurice