Hello experts :)
I just read the schematics of the DAC3484 Evaluation module (http://www.ti.com/tool/dac3484evm)
There is a 6V from Connector regulated to 3.6 (3.3_LDO_IN) and 1.2 with a TPS62420 step down converter.
Then with the 3.6V output of the step down converter 3.3V and 1.2V are created with TPS74201 LDO.
What now is my question: The BIAS Pin of the TPS74201 LDO is not conencted to the 6V power supply but to the 5V of USB. I don't want to use USB so can I use the 6 V of the power supply or is to much "error" on this because it's the Input of a step down converter?
I attached a part of the schematics, I hope this ok, otherwise please delete it!