Hi,
Our customer would like to use TPS54226 on the following condition.
Can they separate VCC from VIN?
I think that it is usable for the recommended voltage range*.
Could you please give us your advice.
*Recommended voltage range (datasheet page3)
VCC = 4.5V to 18V
VIN = 2.0V to 18V
[Condition]
・VCC = 5.0V
・VIN = 2.7V to 8.4V
・Vout = 1.1V
・Iout = 1.5A
Regards,
Kanemaru