Other Parts Discussed in Thread: BQ76940
Hi TI experts,
BQ76940 does not respond to any of the I2C commands. According to the oscilloscope traces, it does not generate ACK signal. (bus is not pulled down in the 9th clock cycle)
I have double verified the I2C connection and 'BOOT' signal is given prior to the I2C communication. Further , voltage at REGOUT is also verified to be at 3.3V.
I tried all the possible address, (0x08, 0x18, 0x00,0x3f) and the result is the same. Finally I2C commands are given using EV2300 module. Again the oscilloscope traces showed the issued signal is correct and no 'ACK' is received.
What could be the reason for not giving the ACK for the address byte?
Thanks,
Ushan Karunathilaka