I wish to connect 2A output of the TPS542941 to clean devices (such as USB) and 3A channel more noisy devices (such as motor driver).
As such, I will need to design two different ground planes as the return path to prevent unwanted noise on clean devices. PGND1 (pin4) will be returned to the clean ground and PGND2 (pin13) will return to noisy ground as shown in below:
Below are my inquiries:
- Could you advise to which ground plane should GND (pin8) pin return to?
- I need to return the body IC to ground as well. Can you also advise to which ground plane should the body IC return to?