Hello
I intend to use the LM5107 in a new design. The circuit topology is relatively straightforward, or so it seems.
I'm looking to swing the common node (source of Q1, drain of Q2) at low frequency from the DC bias point of ~6V to the top rail 12V and then some time later to the bottom rail AGnd then back to neutral. See pic below.
The LM5107 is not working as expected. The high-side fet is not turning on. The data sheet does not state when/how the bootstrap cap is charged and I suspect that's the root of the issue. I've checked layout, part values, footprints etc.. When both HIn and LIn are low, both fets are off as expected and the bootstrap cap (HS pin) sees the 6V bias. When the low side FET is on, the cap sees 0V as expected. The high side FET never turns on and the waveform at HOUT is odd. The bootstrap cap value is 1uF. I tried .47uF as well. The time either FET is 'on' is around 3us, 'off' otherwise.
Any one have any experience with either half-bridge circuits in general or this particular part please?? I don't see why this circuit is so fussy...
Is it the DC bias point causing issues?
Does the cap charge when the low-side FET is on? Or, does it simply follow the voltage on the common node? If that is true, then it should just charge to 12V - 6V = 6V right? Then, the voltage on the high side gate should be the 6V cap voltage + 12V supply = 18V?? The FET should turn on....