Hello All,
I'm looking into doing a Bob Smith termination for a Power over Ethernet (POE) PSE. The TI app note (http://www.ti.com/lit/pdf/slva233) shows the following termination:
But all of TI's reference designs (and later figures in the same document) use the following termination with two ESD capacitors:
Are these circuits equivalent? What is the purpose of having a second ESD capacitor? Doesn't this break the current path between the two 75 Ohm resistors that are supposed to terminate the common mode signals?
Thanks