Hi,
I am using BQ2050 for showing Li-Ion battery capacity indicator as standalone device without any microcontroller. Battery capacity is 1300mAh and using 50mOhm sense resistor. Only first 3 LED's are glowing if the battery is fully charged and 4th &5th LEDs are not at all glowing. PFC settings are given below
PFC Value = 1300*0.05 = 67.5mVh
Approximately choosed PFC = 40960 or 64mVh
Jumper setting for program pins are PROG1 = H, PROG2 = L, PROG3 = H, PROG4 = Z, PROG5 = Z
Please provide me the solutions to debug this issue...
Thanks & Regards
Manikandan J