Hi,
I'm using UC3843 for a Flyback converter, if I load more than 80ma, then output is dropping and reflecting back on the input.
Input Voltage = 100-200 VDC
Output = 24V, 0.5 A
Frequency = 100 Khz
Inductance = 2.3 mH
Output remains 24V as long as output current is < 80ma, but when the load on the output increases, then 12.3 V is there both on input and output.
Thanks,
Amruth