Other Parts Discussed in Thread: BQ76930, BQ78350
Hi, Im trying to build a Battery Management system for 10 Li-Ion battery cells, and Im using a bq76930 for the project. Unfortunately when I try to balance the cells I don't get any balancing current. That means both internal and external balancing(no current). I use exactly the same schematic at page 44 in the datasheet. I use 1k resistors for input resistors. I can read the cell voltages but balancing the cells is not possible. Another problem that Im having is that the external thermistors doesn't work. If anybody knows what this depends on or why there are no balancing currents please wright me back. Thanks.