Hi,
I am having a problem with inrush current using the LM22675.
The LM22675 is set up to provide a 5V Vout from 24V Vin. The output capacitor is 150uF and the output inductor is 330uH.
The inrush current measured using my scope is coming out about 600mA however the load current is only 30mA. It would be good if we could limit the inrush current to less than 150mA.
Are there any ways I can limit the inrush current for this chip?
Thanks in advance for your advice
Regards
Ben