Other Parts Discussed in Thread: LM74610-Q1, SM74611
Hi,
I am working with High side driver ,current of 20A (like 6 drivers) .Now I have to protect the system from reverse voltage,since current is high I cannot connect diode in battery (+) terminal so I have connected the Mosfet (BUKBUK7628-100A) the free-wheeling diode(please find the attached circuit image).
Here my question is Drain is connected to ground , source is connected to free-wheeling diode anode,and gate is connected to 5V supply always,now the MOSFET will work or not?if this is not right method please suggest some circuit.
Later i realized the n channel mosfet is fabricated on p type substrate and source and drain are (n type) sandwiched on P type substrate, Mosfet to conduct more gate voltage is needed w.r.t source .if I apply gate voltage w.r.t to drain(zero Volt)
the channel cannot be formed is my understanding right.?