Hi all,
Would you mind if we ask PG operation of TLV62080?
The datasheet shows as followings;
-The power good maintains high impedance once the output is above 95% of the regulated voltage,
and is driven to low once the output voltage falls below typically 90% of the regulated voltage.
-When the device is off because of disable, UVLO, or thermal shutdown, the PG terminal is at high impedance.
In followings condtion, PG is also Hi-z(High impedance) , isn't it?
-Enable pin : Low(Disable)
-The output(Vout) : over 95%
-Vin: not UVLO(over 2.0V)
Kind regards,
Hirotaka Matsumoto