Building a DC/DC power rail based on the LM27403 with the major driving factor being efficiency. Im looking to achieve over 95% with a 5v power source and .8-1v core voltage output with total load being under 15 amps. Typical load will be between 2-10 amps.
Webench tells me that the LM coupled with CSD16323Q3C /CSD17573Q5B High/low MOSFETS switching 200khz and a 1.3uH inductor with 1.8mOhm DCR will get the job done with over 94% efficiency in my typical load range and 96% at nominal load of 5A.
The LM data sheet (section 9.2.2 and 9.2.5) shows the buck coupled with Power Block NextFETS (which combine high/low mosfets into one). For my application is there a reason to go with the power block route? I don't see any way to generate schematics or simulate efficiencies with these power block mosfets. 9.2.5 shows an example of a "ultra high" efficiency setup using DUAL power blocks for a 5v input rail. Would this "ultra high" efficiency be greater than what webench is showing me for application?