Other Parts Discussed in Thread: UCC28070A, UC2854A, UCC28180
I am looking for a suitable PFC controller for a design receiving three phase power. I desire to implement one boost converter for each phase, followed by a full bridge. Requirements:
-Each phase should process about 1kW.
-The input frequency is 380Hz to about 700Hz.
-The input voltage is TBD depending on whether the PFC stages will be delta connected or wye connected.
-The performance requirements are not super stringent, so a first order cut at active PFC should suffice.
-I want to synchronize the three phases and DC-DC to mitigate beat frequencies.
So far I have narrowed the choices to UC2854A/B, and UCC28070A. Questions:
The UC2854A indicates useability up to 400Hz line with a 5MHz GBW on the currrent amplifier. Can this device do OK at 700Hz? Again, the performance requirements are not super stringent, so a first order cut at active PFC should suffice.
The UCC28070A can provide interleaved functionality which will help with packaging / EMI filtering / dissipation, but does not specify current amplifier GBW or max line frequency. Can you provide the GBW for this device?
Are there any devices more suitable that I have missed?
Thanks!