This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I use LM5085-Q1 to get 13.5V and 10A or 65V and 15A Output at 70V input

Intellectual 750 points

Replies: 0

Views: 88

Can I use LM5085-Q1 to get 13.5V and 10A or 65V and 15A Output at 70V input