Hi,
I do use the TPS61045 in a circuit.
Input from 3 to 4 V aprox. Output 8 or 15V.
When the output is set to 15V, the output is good.
When using 8V, some devices have a correct signal and some of them have some spikes that generate problems in some measurements.
Can anyone give a clue of what could produce this behavior is some devices and not in others? Any clue of which part could introduce this noise?
Thanks