What is the lowest output voltage for the TL5209. I'm looking for a low drop-out linear regulator that can handle 2.5V in and put out 1.2 - 1.25V at up to 200mA. I'm using the TL5209 in another part of this design, so even though it is overkill for this particular function, it will be simplify the BOM and increase buying efficiency. According to the info on Page 15 of the data sheet, it appears that if R2/R1 approaches zero, it should put out 1.242V, but I'm not sure how low R2 can go, and what the ideal value of R1 would be in that case.