Hi,
i am having trouble with my application. Built as shown on the attached schematic, my input power supply (which is rated at 3A) goes into shutdown mode when I try to turn on the power. i believe the transistor M1 is always on. the transistor being used is a IRFB4710. I have also tried various gate resistors.
I also noticed the input filter RC note. Does this RC filter also tie to the inductor or should that side be directly connected to Vin? What are some good starting point values for the low pass RC filter?
Thank you ,
Gary