Hi,
Could you please help to review schematic of TPS22954 as attachment.
Vin=3.3volt
Vout=3.3volt
Enable threshold: 3.0volt.
Output power good threshold:3.0volt.
Thanks!
Jefer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you please help to review schematic of TPS22954 as attachment.
Vin=3.3volt
Vout=3.3volt
Enable threshold: 3.0volt.
Output power good threshold:3.0volt.
Thanks!
Jefer
Hi Jefer,
The schematic looks good and it seems that both the enable and power good have been set to 3V based on the resistors chosen..
Thanks,
Alek Kaknevicius
Hi Jefer,
When turning on this should not present a problem since the enable is the only one looking for a 3V signal. VOUT is not yet up at this time, so the sense pin does not "conflict" with the enable pin.
When turning off, because both are set to the same threshold, either one may trigger. However, both will accomplish the same thing: PG will be pulled low and the device will be turned off. The difference is that the sense pin going low will restart the device while the enable pin going low will shut off the device completely.
Can you give me a bit more information on the application? Why do both sense and enable need to be set to the same 3V level?
Thanks,
Alek Kaknevicius