Can I use the TI LMZ14201H type SIMPLE SWITCHER MODULE (or, more generally, all of the SIMPLE SWITCHER MODULES including the high-density Nano Modules --e.g. LMZ21701) in an inverting configuration to create a negative voltage output?
Thanks,
Tom
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use the TI LMZ14201H type SIMPLE SWITCHER MODULE (or, more generally, all of the SIMPLE SWITCHER MODULES including the high-density Nano Modules --e.g. LMZ21701) in an inverting configuration to create a negative voltage output?
Thanks,
Tom
There are many who know this more than me, but the LMZ14203 is a step-down DC-DC converter. If you apply 12V you can only create something less than 12V (in fact, they say 9V by saying the Vin should be at least Vout + 3VDC). It is possible to level-shift the 9V so that it runs from 0 to -9V (instead of the more typical 9V to 0), but you will still only create an output voltage difference of up to 9V.
If you need to get a larger voltage than what you start with, you'll need a "boost" DC-DC converter.
Hope this helps...
Tom
Thank you for the clear explination.
So in negative configuration +12V in gets -15V out, @ 2Amp in stead of 3Amp.
in negative mode maximum operating input voltage will drop from 42V to 42-15V = 27VDC
Learn from mistakes:
In a design i made a mistake, there are used 2 LMZ14203H to create +15V and -15V that supply some high current opamps.
The circuit is supplied with 12VDC.
Now the problem is, what was supposed to be +15V = +12V because LMZ14203 output cannot be higher than the input.
Solution increase the supply voltage.