Hello,
I am attempting to design a high-voltage constant-current supply based on the UCC28701 controller. The final application will be a simmer supply for a laser flashlamp. Here are the supply specifications:
24VDC input
300V open-circuit output
300mA regulated output current
I have followed the design guidelines given in the various application notes, mostly in TIDA-00182 (www.ti.com/.../tida-00182). Here is the schematic I'm currently working with, and a photo of the setup.
imajeenyus.com/.../full_schematic.pdf
http://imajeenyus.com/temp/simmer/IMG_9766.JPG
The transformer is wound on a gapped ETD34 core and has about 1:13 winding ratio. Note that I am taking the voltage sense feedback directly from the secondary winding, since there is no requirement here for an isolated supply. It saves having a separate auxiliary winding.
Before you recoil in fright at the photo of my test setup, yes, I am aware that "dead bugging" switchmode supplies is far from ideal and causes lots of problems with stray inductance. However, that issue is not really relevant at the moment.
Essentially, the UCC28701 refuses to do anything at all, period. There is no gate drive output, not even a few pulses on startup. I would've thought that, even if the feedback components were not quite right (which, having double-checked the calculations, I'm pretty sure they are), it would still do something. The actual power side of the circuit works perfectly - if I drive the MOSFET "manually" from a signal generator + gate driver chip, I can get the specified voltage and current at the output. The feedback waveform looks excellent, with very little ringing.
I have left the NTC input open, which I think is correct, so it's pulled up and doesn't shut down the chip.
I am really at a loss what to do next, and would appreciate any advice. Is there something I'm completely missing about the operation of this chip?
Many thanks,
Lindsay Wilson