Other Parts Discussed in Thread: LM1084, LM317-N, LM337-N, LM1086, LM340
Hello,
We have two inputs: +15V, -15V and a common, we need to use two LM1084 to generate +12, -12V and a common. Could we connect the two LM1084: U1, U2 in the following:
1) Input of U1 is connected to +15V, GND of U1 is connected to Common; and output of U1 outputs +12V;
2) input of U2 is connected to common, GND of U2 is connected to -15V; and output of U2 outputs -12V.
Best regards,
Mark