This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 465
Hi there!
we are using TPS7A4901 in this condition : Vin=14.4V~19V, Vout=12V, Iout=80mA. Css=CFF=10nF.
On page 17 of datasheet, it says Cout has to be larger than 2.2uF and Cout(max) should also be limited by equation(7) and (8). I am confused:
Why tss(CL) is 140us and Vout =2V in equation(8)? I thought Vout should be 1.2V as page 16 wrote...
And in my application, Cout(max) = 140us*500mA/12V = 5.83uF. This seems to confilcts with the requirement that "Cout could use 10uF for better PSRR"?
So how should I choose Cout?
Thanks!
In reply to Mark Sellers:
In reply to XY:
Hi Mark,
datasheet section 8.3.1 says "For reliable operation, the device does not operate in current limit for extended periods of time", is this "time" specified as less than two decades below tss(1/100 of tss) ?
What will happen if current limit is reached but other condition is good for Table1? will the IC shut down?