Hello all,
I have a unit with following input power supplies: (1) +7V with 0.4A, (2) +5V with 0.2A and (3) -5V with 0.06A.
I have to switch-off the unit with a DO from a controller. This controller is operating on a separate power supply.
Any of the CSD13302W, CSD13306W, CSD13383F4 or CSD83325L will suite for my application? Further any driver device is required?
Can anybody suggest me the suitable circuit please?
Thanks in advance.