I'm having an issue with a recent board layout, and I'm not sure if I misunderstood the functionality of the IC or if something else is going on.
When battery voltage is applied to the board (single-cell LiPo), the battery voltage passes through to the output even when the EN pin is pulled low. My understanding from the datasheet was that the input/output are disconnected in shutdown mode.
Is this normal behavior or am I missing something? Pictures of the layout/schematic below.