Dear sir,
I am using TIS LP55281 in our product with I2C communication.
In the datasheet
1) Typical application connection diagram does not mention any connection for "NRST" pin. can I left this pin un connected in my design? Will the IC get proper reset?
2) "Modes Of Operation" section on page 8 mentions about RESET as "The LP55281 can be reset by writing any data to the Reset Register (address 60H). " Does this means that even I left the NRST pin unconnected and write random value at 60H will reset the module? I want to understand, before I write at address 60H using I2C, in what state LP55281 is?
3)Please confirm, whether writing at address 60H will bring chip in reset state after powering oN my device or it will reset the chip at any point during its normal operation?
4) The block diagram shows connection of LP55281 with microcontroller, here along with I2C lines , NRST is also connected to MCU. Why?
As NRST is active low, does this mean that we have to connect this pin to provide reset signal at power ON.
5) It will be great if you can share some code for I2C interface of LP55281 as an example.
6) Please confirm whether, NRST should have connection for Active low signal or only writing to address 60H will provide reset to pin?
Regards,
Sujata