I am looking for a solution (PFC + Flyback) topology. This is a universal input, 100 watts, 15V output. I need low ripple at the output, So I can not use UCC38050. I am looking a solution with a separated inductor for the PFC (separated from the main flyback transformer. This way, I can filter the line frequency at the output of the PCF and obtain a 15V output with low ripple. Does TI has a chip with this characteristics? Thank you Victor Castrellon