Hi,
Read the datasheet, the LMZ10500 can output 0.6V ~ 3.6V from input 2.7V ~ 5.5V. On the P.19 (application section), the Fig.32 provides output 3.3V with Vin. I'm not sure whether it means the IC can output 3.3V even if input voltage 2.7V. Similarly, can the chip output 3.6V from input 3.0V?
Thanks,