Hello,
One of my customer found the below behavior with LM26003 at light load. I guess the Frequency Foldback is wroking here. However, there are a lot of things unexplained. Please make an answer to each question below, or if my guess is totally wrong, please give me some insight.
In the below figure, an experiment of VFB pulled to GND is shown. Yellow shows Vout while red shows VFB. Vin is 13.5V, Vout is configured 5.0V, and the load is 1kohm resistor.
At the left end in the figure the device is in stable operation at Vout = 5.0V and Vfb = 1.236V.
When VFB is pulled to GND at the first grid, Vout changes from 5.0V to somewhere above 6.0V.
Q1: Do you think the Frequency Foldback limits the Vout at around 6V?
Then, some noise injected to VFB triggers Frequency Foldback to discontinue making Vout close to Vin.
Q2: Does an increase in Vfb release Frequency Foldback?
Another strange behavior not shown in the figure is that Vout settles to 0.0V long after pulling VFB to GND. You should see in the figure the descending Vout. It eventually goes to GND after a long while.
Q3: Do you think this is a valid behavior?
Thanks.
Regards,
Oguri (TIJ automotive FAE)