Hi,
For an handheld system I use a TPS564208 to get 3.3V from a 7.4V Li-Po battery. To test it I used a laboratory power supply. Actually on my PCB I have only the TPS564208 and its necessary capacitors, resistors and 2.2uH inductor.
Problem (or not?), even with no load, it consumes about 25mA... As it is will be used as a permanent supply for the system (low power MCU), it will be a big problem for battery lifetime...
To get 3.3V I set the reference resistors to 33.2k and 10k.
I tried to change 33.2k to 332k and 10k to 100k but the cunsumption was worse, about 70mA...
I used this one because I thought it would be better than an LDO to go down to 3.3V with a 7.4V supply.
Do you know if it's a normal case or if I did something wrong? Is there a better device to do it?
On this rail I need only 20mA (Low power MCU + 1 LED)
I also have two other rails which can be enabled or disabled by the low power MCU (3.3V 250mA and 5V 1.5A)
Thank you.
Regards,
Loic