Other Parts Discussed in Thread: AM3351
.Hi,
I am using PMIC TPS65910A3A1RSLR in the design with AM3351.
I have below queries
a. This PMIC has Vbackup pin and if coin cell battery of 3V is connected to this pin. Can i read the time from the serial port available in this IC?
b. in the boot mode Boot1=1 (High) and Boot0=0, (gnd), what are the output voltages in DC DC outputs and LDO's?
Thanks in advance
Regards
Sujay A