关于PMP7282,LM5116最大输出电流参数是20A,为什么PMP7282中参考电路输出回事25A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The value in the table is some kind of recommendation. Assuming appropriate inductor and external MOSFET, it's always possible to push output current to 20A above.
For a controller, because the external components are selectable, we don't quite often talk about the maximum current. If you read the datasheet of LM5116 carefully, you can find that there is no such information about maximum output current because it is periphery depends. The limitations of maximum output current are often thermal consideration and current sense resistor.
Hope it helps.
Thanks.