This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 699
Part Number: UCC2808A-1
Is it possible to achieve a circuit of Fig.2 of ucc2808 data seat?The input voltage area which is 72V from 36V by Push - Pull system, can it correspond?
In reply to John Stevens:
John-san
I'm seeing rebesion SLUS456D of a dataseat.
The circuit which is being asked is attached.
Best Regards,
In reply to Hirotsugu Kobayashi:
In reply to John Griffin1:
Hi Kobayashi-san,
The push pull can be designed for this wide voltage range.
For example if the output duty cycle is 90% at 36V (corresponding to 45% duty cycle on each gate drive) then the required output duty cycle will be 45% at 72V(corresponding to 22.5% duty cycle on each gate drive)Does that make sense? Of course it is always difficult to design a power supply with a wide input range but it is possible to do so with the right care and attention to details
Regards,
John