Hi.
I used the LM5116,designed it,and created a prototype.
The design parameters are as follows.
Vin: DC18-30V
Vout:DC16V/13Amax
Chf:33pF,Rcomp:56k,Ccomp:270pF( form LM5116_quickstart.xls)
Rcramp:240k,Cramp:820p
Rs 2mohm,Fsw:100kHz
Q1.Increase the load(0->13A),Switching operation stops at about 7A.Why?
Current limit::55A? I hope I can output 13 A or more.
Q2.Is there a way to disable the current limit function?
Q3.Reducing the value of Rcramp made it possible to flow a large current.Why??
I am very embarrassed. I am waiting for an answer.
Best regards.