This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: Learning Cycle Failure

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi,

I am using BQ27542-G1 gas gauge for battery charge monitoring and facing issues in learning cycle. Below are the two tries which I have done.

In the first attempt, The discharging phase completed successfully. We had kept for relaxing. During relaxing period, after some time, we got an error message “RUP_DIS/RDIS: Not clear” and learning cycle cancelled.

In the second time, it failed during relax time after charging cycle completed. In the "Updated Status" it was changed from 04 to 05. But we got an error : (VOK : Not clear).

Please find the attached  images for the reference.

Please help to understand why this failure happening.

Can I get the exact flow of the entire process. Below mentioned is the flow which I have done.

  1. Selecting the Chemistry ID ( Selecting Default)
  2. Calibration (CC and Voltage)
  3. Setting Parameters Q & A
  4. Starting Register Logging and Data Memory Logging. ( Observed that logging does not happening sometimes. Sometimes Learning cycle is not starting if logging enabled)
  5. Starting Learning Cycle. Observed that discharging is happening always at around 800 mA current irrespective of the load which I am using. 

Please correct if the procedure which I am following is wrong.

Regards,

Vipin N N