Other Parts Discussed in Thread: AM5728
Tool/software: Linux
I am now in the development of AM5728, PMIC is not working properly, the use of TPS6590376ZWSR chip, SMPS9 3.3V output is not working now, the measured voltage is 1.37V (voltage may be peripheral leakage over the other SMPS), the output voltage is normal (only +VDD_MPU SMPS1, +VDD_DSP SMPS5, do not work).
I use the 5V supply that reference schematic, the need to use TPS6590377ZWSR?
The following is my PMIC schematic