This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 272
Part Number: TPS62400-Q1
Hi There,
For the TPS62400-Q1 what is the maximum (low ESR, ceramic) capacitance that can be placed on output 1 of a TPS62400-Q1, when it’s set to 1.2 V and has a 2.2 uH inductor?
Does it matter if it is set for permanent PWM or if it’s allowed to go to PFM mode?
Thanks in advance for your help.
Regards,
Ross
Chris Glaser
Texas Instruments
________________________________
TPSM82810 - new, 6Vin, 4A, high efficiency power module with clock synchronization Now sampling!