This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82084: behavior of Power Good

Part Number: TPS82084
Other Parts Discussed in Thread: TPS82130

Hi,

We got a question from customer about TPS82084.
Could you help us?

[Question]
Our customer consider to pull up EN and PG to Vin.
What is behavior of Power Good at each condition A to F in below figure?

Best Regards,
tateo

  • Section 8.4.2 in the D/S explains the PG behavior under various conditions. 1 clarification to this description is that 'UVLO' should instead be 'Vin removal'. Table 1 in the TPS82130 D/S shows a more precise explanation of the PG behavior, which also applies to the TPS82084.

    Specifically for your drawing (with EN = Vin), A and F will show PG at the Vin level, while other regions will hold EN low. But A and F should be re-labeled based on the Vin level and will occur around 0.7Vin.