This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27524A-Q1: "RNMOS, Pull Up" On resistance value

Part Number: UCC27524A-Q1

Dear all,

My customer want to know that each 3 FETs gate pulse width and mutual phase
of datasheet P14 Figure 20.

Because ROH= Pch is 5 ohms it's too BIG,
and no description about parallel "RNMOS, Pull Up" on resistance value.

Thank you.

  • Hi Doi-san,

    I have asked one of the HPD engineers to respond to your question, you should see a response soon.

    Regards

    Peter
  • Doi-san,

    In the UCC27524A-Q1 device, the effective resistance of the hybrid pullup structure during turnon is estimated to be approximately 1.5 × ROL, based on design considerations. Taking the spec for ROL from the Electrical Characteristics table, the estimate for the effective resistance of the hybrid pullup structure during turnon, including the parallel "RNMOS, Pull Up)" is:

    PARAMETER TEST CONDITIONS MIN TYP MAX UNIT
    Effective resistance of the hybrid pullup During turn-on 0.225 0.75 1.5

    The NMOS pull-down (ROL) and the PMOS pullup (ROH) have complimentary behavior. For low-to-high output transitions, ROH and RNMOS,pullup turn on at effectively the same time, with RNMOS,pullup staying on for only a short pulse. I will consult with the IC designer on the duration of the pulse, but please note this may be TI proprietary information and I may not be able to share.

    I do hope that thispost has helped address your question. If it has, please press the "Verify Answer" button below.

    Regards,

    - Daniel

  • Daniel-san,

    Thanks!
    I an now waiting for customer's reply.
    If T inc. and Customer contract NDA, proprietary information can be open? May be No.
    If Effective resistance of the hybrid pullup spec is in the specsheet, more customer use this.

    Thank you,

    H.DOI